Hi,
I want to implement SPI0 and SPI1 interface on BBB but first SPI0.
What exact modifications do I need to do to run the mcspiFlash.c on SPI0 of beagle bone black? I can change the header file to beaglebone.h in place of evmAM335x. I can change the platform library. Do i need to modify the functions McSPI0ModuleClkConfig() McSPIPinMuxSetup() and McSPI0CSPinMuxSetup() at all for SPI0
here is one post which gives a hint but why these functions require a change of above functions for SPI0??
Regards..