Hello guys !
I'm currently building a project of my own with my board : ICE v2 AM3359.
It's running with SYS/BIOS SDK (SYSBIOSSDK-IND-SITARA) using StarterWare example based UART communication.
Now, I need to add DCAN functionality to my project.
For that, I'm trying to use the dcanTxRx example from AM335X_StarterWare_02_00_01_01.
I can build it correctly but I won't work on my board. Do you have an idea why ?
What's the best way to incorporate DCAN to my project ? Maybe using only SYS/BIOS StarterWare example files ?
Do I have to be careful with the compiler I use ?
Regards,
Nicola De Lellis