TI Starterware support Team,
My customer uses Starterware for AM335x platform.
-Issue:
When USB memory inserts to their system with AM335x,
the babble faults appear.
-Details:
*occurrence rate; about 1%, but once this babble fault occurs,
it does not recover with re-inserting USB memory.
*The usb memory is specified by customer and never occured this error so far.
-Quastions:
1. This babble fault is same as babble interrupt in Linux?
I just refer the following post.
https://e2e.ti.com/support/embedded/linux/f/354/t/484475
2. If "Babble fault" is "Bubble interrupt", does the babble fault occurs
when the hots(AM335x) receives more data than the specific maximum packet size?
3. Are there any work around for this issue with Starterware?
In this community site. there are some workarounds such as the patches for Linux,
or using USB hub.
However my customer can not change their board design,
so they would like to fix this issue by softwate; means starterware.
Best regards,
Kanae