Hello,
I have a configuration issue with my project. I am using NDK1.7 in ccs2.20.18. When heap was set more than 24MB, the NDK can only working on 1.5MB/s.When heap was set small than 24MB, the NDK can working on11.5MB/s. Why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Zuxin,
Which hardware platform are you using?
Could you attach the memory map file for your project? It will have a ".map" extension.
Also, the NDK and CCS you are using are *very* old. It is possible that you are hitting some bug in NDK 1.7 that has been fixed in a later version.
Thanks,
Steve