Hi,
My algorithm is not qualified by QualiTI (XDAIS Rule 8 - Namespace compliance):
Test failed. Problem: Not all global symbols defined by the module have the "IRCOMP_HEXIUM_" prefix (i.e. module_vendor_).
This because, there are several C functions in separate source files.
These functions are locals in the library and they will be never call from the outside (e.g. by an application).
But, I cannot use "static" keyword because these are placed in separate files.
I tried the "#pragma FUNC_NO_GLOBAL_ASG(func)" but it won't help.
How can I link my internal functions as library-local?
Best regards,
Peter
PS: Tools versions:
CCS: 5.3.0.00090
XDC: 3.24.05.48
CGT C6K: 7.4.1
XDAIS: 7.21.01.07
QualiTI: 7.20