When we use System-Analyzer with loggerSM (shared memory, no cashed) the DSP load increases
massively (more than 10%). Also we could see that the most additional load is produced if
sysbiosTaskLogging is on. The number of the sysbios task events runs up to 21000 events per second.
Is the load so big because of to many events or can it be a configuration problem?
Is it possible to deactivate the logging of some specific sysbios events, for example Task_LM_setPri?