hi everyoen
Locate the file or edit the source lookup path to include its location."
clould you give me some advice how to write drivers,and How to deal with this bug.
thanks
aria li
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi everyoen
clould you give me some advice how to write drivers,and How to deal with this bug.
thanks
aria li
Aria,
you need to direct the debugger to the location where you have installed the Sys/Bios files. The sources are there and then you can debug the issue. Above is not the debug output but a message by the tool that it can't find sources. This is usually the case if libs are built on another machine and contain the absolute paths.
Otherwise there is a dedicated Starterware forum.
regards,
hi
console prints this information
[CortexA9] Exception occurred in ThreadType_Main.
Main handle: 0x0.
Main stack base: 0x8001e350.
Main stack size: 0x1000.
R0 = 0x44df2b48 R8 = 0x48040000
R1 = 0x00000003 R9 = 0x00000000
R2 = 0x00000000 R10 = 0x0003ba80
R3 = 0x44df2b48 R11 = 0x8001f274
R4 = 0x00000001 R12 = 0x8000e6c4
R5 = 0x800139ac SP(R13) = 0x8001f258
R6 = 0x00000001 LR(R14) = 0x8000e9f4
R7 = 0x8001f350 PC(R15) = 0x8000e6e4
PSR = 0x600001df
DFSR = 0x00000005 IFSR = 0x00001000
DFAR = 0x44df2b48 IFAR = 0xbed5eead
ti.sysbios.family.arm.exc.Exception: line 180: E_dataAbort: pc = 0x8000e6e4, lr = 0x8000e9f4.
xdc.runtime.Error.raise: terminating execution
clould you give me some detailed advice
thanks
aria li
Aria,
no, as we can't guess what code you have here: E_dataAbort: pc = 0x8000e6e4
You really need to single step through this and figure out what is happening. Hint: usually it is some kind of peripheral that has not been enabled (clocked). So ARM can't access the registers and will throw an exception.
Regards,
Aria,
aria li said:am437x "StarterWare_02_01_00_02"
I don't think this is a public release. At least I can't find it on our web pages. So you should ask the person who gave this to you for support. We can't discuss early engagements on the public forum.
Regards,