Hello,
I'm using the CCS v6.0 of Eclipse and I work on a logger subject.
I'm retrieving logs from my DSP and then create a binary file with all my logs. What I want to do is to open my binary file via System Analyzer. So I do "Tools/System Analyzer/Open from binary" and it should open a window where I have to put my different file and folder (.bin, .out, .uia.xml...) repositories before launching the System Analyzer session.
At first I had no trouble launching a system Analyzer session following these previous steps. But for an unknown reason, opening the "open from binary" window doesn't work anymore. In fact it displays the "Progress Information" window where you can see the load of "Discovering analysis activities", then this window disappear and instead of opening the "open from binary" window, nothing happen.
I tried to relaunch CCS several times, I tried to connect my evaluation module board, I also tried to open it with the CCS v5.5 from another computer and I noticed the same problem.
If someone could give me a hand on this issue it would be great?
Thanks,
Nad