I do an experiment on ccsv5,on which I run an openmp program ,but I met some questions ,please help me.
1.I run the Helloworld example on custom board not on the EVM, the project could run successfully on simulator , but failed on emulator,with the mistake ipc_attach ,and how to solve it?
2 How can we run openmp on our custom board,and by which means can we root the openmp ,and whet is the openmp's root process?
3 . I used the ti.omp.examples.platforms.evm.6678 ,and what is the relationship between it and ti/omp-1-01-03- 02/packages/ti/omp/platform/evm6678? Namely,how can we gain our generic platform accodring to the modifying of the EVM platform ?
4.I want to know how to modify the platform ,and I want to use our own custom board . Because the DDR’S address range on evm is from 0x80000000 to 0x9fffffff,but on our custom board is from ox80000000 to 0xffffffff . And the beginning address of the MSMSRAM_Nocache on EVM is oxa0100000,but on the custom board is 0x50000000.How to modify the platform based on our custom board ?
5.The tools I used are as the following
Compiler version :TI v7.4.1
IPC :1.25.0.04
MCSDK PDK TMS320C6678 : 1.1.2.6
OpenMP BIOS runtime library:1.1.3.0.2
SYS/BIOS :6.34.2.18
Are there problems about the tools I used?
I am very appreciated with your early reply.