I'm trying to import and rebuild "uartecho" demo application for AM3359 ICE demoboard.
I've followed these instructions: processors.wiki.ti.com/.../AM335x_SYSBIOS_Industrial_SDK_Getting_Started_Guide
The software requirements reported in the same page are:
AM335x Industrial SDK Code Composer Studio version CCS 6.0.0.00190 SYSBIOS 6_40_03_39 Real Time Operating System Network Development Kit (NDK) 2_24_00_11 Serial console terminal application (like Teraterm, minicom, HyperTerminal)
So I've installed everything accordingly:
- SYS/BIOS: bios_6_40_03_39
- XDC tools: xdctools_3_30_04_52_core
- CCS: 6.0.0.00190
- am335x_sysbios_ind_sdk_1.1.0.6
In a machine running Windows Xp and Java 1.8 32 bit everything works fine.
In a newer machine running Windows 7 and Java 1.8 64bit with exactly the same software installed I can't view or edit .cfg file
No [SYS/BIOS] appears on the right of the uartecho.cfg file in project viewer panel, and double clicking on that file nothing happens:
Closing the empty box in editor panel this error window pops up:
VERY, VERY, VERY, VERY FRUSTRATING.
HINTS?