Board DK-TM4C129X.
Controller: TM4C129NCZAD
OS - TI-RTOS 2.12
CCS 6.1 (using Free License as we awaiting the license) and TI ARM Compiler 5.24
We are having an application with multiple Tasks (totally 5). All are running with same priority. Two tasks are used to read from peripherals and 1 task is used to send data over the same peripherals. Other tasks are the display task to display on LCD. The core task (core functionality) is 5th task. MailBox is used to sync data between tasks.
We are facing a peculiar problem where in the application is crashing in the display task. We have ensured stack size is OK. While analyzing the crash, we see that commenting random part of code with substantial lines of code, either in display task or the core task The application does not crash. This seems to some sort of code size issue, Is there any limit on the code size?