I'm running into an exception in the code section: ti_sysbios_utils_Load_updateCurrentThreadTime__E. I believe this is the module which is causing the exception because when the exception is hit, the PC lies within the code range for that module. I have several LOG_print function calls throughout my application, and if I conditionally compile them all out, I do not hit the exception. Also, if I move the location in my code of some of the LOG_print function calls, I do not hit the exception.
I'm having difficulty finding ways to track this down, as I do not have a call stack upon hitting the exception. Upon searching the forums, I thought that the Extended Trace Buffer (ETB) utility would be useful; however, I believe I have found that it is not available on the C6748.
I'm running on a C6748, with CCS 6.1 and SYS/BIOS 6.40.1.15. I am using the XDS100v3 JTAG emulator.
Any ideas on how to track down what's leading to the exception?