Hi at all,
I'm running into some problems. I want to share some data between the c28 am M3 on my F28M35H52C1 Controller.
I create a new Projekt for the M3 and implement a IPC Messaging to share Data between my M3-Project and the SolarExplorer_PVInverter C28Part out of the ControlSuite (controlSUITE_INSTALL_DIR\development_kits\SolarExplorer_v1.1\SolarExplorer_PVInverter_F28M35Hx\C28x). This works very well.
So I create a new Project for the C28 an implement a IPC Messaging and an LED Blinking.
But my M3 and C28 Programms do not share any Data. Both Programms are running . The M3 display some text at the console and the LED, controlled by the c28 are blinking. I think there is something missing in my C28 Project.
Can someone explain me what's missing or what I'm doing wrong?
At the Line 536 to 540 in empty.c in the M3-Project there are some read and write operations through shared Memory.
At the line 198 to 202 in main.c there are the read an write operations in the C28-Project.
The CMD-Files are copies from the SolarExplorer_PVInverte.
I'm using CCS V6.1.3.00033
Thanks an best regarts Chris