Hello All,
I have recently had some strange linking errors while working on a large TI-RTOS project, for the tm4c1294xl launchpad. Everything was working fine, everything compiled ok, until I started getting frequency out of range errors. I reset my workspace by deleting the .metadata folder (and backing it up as well). Long story short, it was caused by a fault in an add on circuit I had, and removing this add on fixed the problem. As such, I restored the backup of my .metadata folder, did a compile / deployment check, and since everything worked, I shut down my computer and went to bed for the night.
When I restarted CCS the next morning and opened my project the next morning, I made a few small changes to the code, added a few lines pertaining to the PWM peripheral, and compiled. It was missing some symbols from the xdc tools timestamp module, so I #included the timestamp.h file, and added the module in the BIOS configuration. When I compiled again, I received an enormous amount of linker errors, stopping only after the 100 error limit was reached. All of them had something to do with BIOS symbols from the .obj files in the TI-RTOS libraries being redefined by those in the "src" folder auto-generated when creating RTOS projects, which isn't even included in compilation normally. I deleted the "src" folder entirely and recompiled. The folder was recreated and I got the same results.
I tried to reset the workspace again and deleted the new PWM code, with the same results.
Any help would be most appreciated,
Brian Duemmer
System Specs:
OS: Windows 7 64bit
CCS version: 6.1.3.00033
XDCTools version: 3.32.0.06_core
TI-RTOS version: 2.16.1.14
TivaWare version: 2.1.2.111
Build Log:
Project source:
**** Clean-only build of configuration Debug for project LinearDeltaCode_v2.0 ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k clean cleaning ../src/sysbios ...DEL /F "../src/makefile.libs" "LinearDeltaCode_v2.0.out" "configPkg\linker.cmd" "configPkg\compiler.opt" "LinearDeltaCode_v2.0.hex" DEL /F "empty.d" RMDIR /S/Q "configPkg\" DEL /F "EK_TM4C1294XL.d" DEL /F "EK_TM4C1294XL.obj" "empty.obj" Could Not Find C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\../src/makefile.libsCould Not Find C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\Debug\LinearDeltaCode_v2.0.outCould Not Find C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\Debug\LinearDeltaCode_v2.0.hex'Finished clean'' '
**** Build Finished ****
**** Build of configuration Debug for project LinearDeltaCode_v2.0 ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all 'Building file: ../empty.cfg''Invoking: XDCtools'"C:/ti/xdctools_3_32_00_06_core/xs" --xdcpath="C:/ti/tirtos_tivac_2_16_01_14/packages;C:/ti/tirtos_tivac_2_16_01_14/products/tidrivers_tivac_2_16_01_13/packages;C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages;C:/ti/tirtos_tivac_2_16_01_14/products/ndk_2_25_00_09/packages;C:/ti/tirtos_tivac_2_16_01_14/products/uia_2_00_05_50/packages;C:/ti/tirtos_tivac_2_16_01_14/products/ns_1_11_00_10/packages;C:/ti/ccsv6/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M4F -p ti.platforms.tiva:TM4C1294NCPDT -r release -c "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5" --compileOptions "-mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path=\"C:/CodeDirectory/CCS/LinearDeltaCode_v2.0\" --include_path=\"C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b\" --include_path=\"C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix\" --include_path=\"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include\" -g --gcc --define=ccs=\"ccs\" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on " "../empty.cfg"making package.mak (because of package.bld) ...generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...configuring empty.xem4f from package/cfg/empty_pem4f.cfg ...generating custom ti.sysbios library makefile ... Starting build of library sources ...making C:/CodeDirectory/CCS/LinearDeltaCode_v2.0/src/sysbios/sysbios.aem4f ...gmake[1]: Entering directory `C:/CodeDirectory/CCS/LinearDeltaCode_v2.0/src/sysbios'clem4f C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/BIOS.c ...asmem4f C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M ...asmem4f C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/family/arm/m3/Hwi_asm_switch.sv7M ...asmem4f C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/family/arm/m3/IntrinsicsSupport_asm.sv7M ...asmem4f C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/family/arm/m3/TaskSupport_asm.sv7M ...arem4f BIOS.obj m3_Hwi_asm.obj m3_Hwi_asm_switch.obj m3_IntrinsicsSupport_asm.obj m3_TaskSupport_asm.obj ...gmake[1]: Leaving directory `C:/CodeDirectory/CCS/LinearDeltaCode_v2.0/src/sysbios'Build of libraries done.clem4f package/cfg/empty_pem4f.c ...'Finished building: ../empty.cfg'' ' 1 file(s) copied.making ../src/sysbios/sysbios.aem4f ...gmake[1]: Entering directory 'C:/CodeDirectory/CCS/LinearDeltaCode_v2.0/src/sysbios'gmake[1]: Nothing to be done for 'all'.gmake[1]: Leaving directory 'C:/CodeDirectory/CCS/LinearDeltaCode_v2.0/src/sysbios''Building file: ../EK_TM4C1294XL.c''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="EK_TM4C1294XL.d" --cmd_file="configPkg/compiler.opt" "../EK_TM4C1294XL.c"'Finished building: ../EK_TM4C1294XL.c'' ''Building file: ../empty.cpp''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="empty.d" --cmd_file="configPkg/compiler.opt" "../empty.cpp""../empty.cpp", line 55: warning #179-D: variable "x" was declared but never referenced'Finished building: ../empty.cpp'' ''Building file: ../source/FileIO/GlobalData.cpp''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="source/FileIO/GlobalData.d" --obj_directory="source/FileIO" --cmd_file="configPkg/compiler.opt" "../source/FileIO/GlobalData.cpp"'Finished building: ../source/FileIO/GlobalData.cpp'' ''Building file: ../source/FileIO/config.cpp''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="source/FileIO/config.d" --obj_directory="source/FileIO" --cmd_file="configPkg/compiler.opt" "../source/FileIO/config.cpp"'Finished building: ../source/FileIO/config.cpp'' ''Building file: ../source/FileIO/inih-master/cpp/INIReader.cpp''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="source/FileIO/inih-master/cpp/INIReader.d" --obj_directory="source/FileIO/inih-master/cpp" --cmd_file="configPkg/compiler.opt" "../source/FileIO/inih-master/cpp/INIReader.cpp"'Finished building: ../source/FileIO/inih-master/cpp/INIReader.cpp'' ''Building file: ../source/FileIO/inih-master/ini.c''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="source/FileIO/inih-master/ini.d" --obj_directory="source/FileIO/inih-master" --cmd_file="configPkg/compiler.opt" "../source/FileIO/inih-master/ini.c"'Finished building: ../source/FileIO/inih-master/ini.c'' ''Building file: ../source/GcodeEngine/GCline.cpp''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="source/GcodeEngine/GCline.d" --obj_directory="source/GcodeEngine" --cmd_file="configPkg/compiler.opt" "../source/GcodeEngine/GCline.cpp"'Finished building: ../source/GcodeEngine/GCline.cpp'' ''Building file: ../source/io/pinout.cpp''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="source/io/pinout.d" --obj_directory="source/io" --cmd_file="configPkg/compiler.opt" "../source/io/pinout.cpp"'Finished building: ../source/io/pinout.cpp'' ''Building file: ../source/motion/DeltaAxis.cpp''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="source/motion/DeltaAxis.d" --obj_directory="source/motion" --cmd_file="configPkg/compiler.opt" "../source/motion/DeltaAxis.cpp"'Finished building: ../source/motion/DeltaAxis.cpp'' ''Building file: ../source/motion/DeltaKinematics.cpp''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="source/motion/DeltaKinematics.d" --obj_directory="source/motion" --cmd_file="configPkg/compiler.opt" "../source/motion/DeltaKinematics.cpp""../source/motion/DeltaKinematics.cpp", line 36: warning #2337-D: list initialization syntax is a C++11 feature'Finished building: ../source/motion/DeltaKinematics.cpp'' ''Building file: ../source/motion/PID.cpp''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="source/motion/PID.d" --obj_directory="source/motion" --cmd_file="configPkg/compiler.opt" "../source/motion/PID.cpp"'Finished building: ../source/motion/PID.cpp'' ''Building file: ../source/util/VecMath.cpp''Invoking: ARM Compiler'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/CodeDirectory/CCS/LinearDeltaCode_v2.0" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b" --include_path="C:/ti/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/packages/ti/sysbios/posix" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on --preproc_with_compile --preproc_dependency="source/util/VecMath.d" --obj_directory="source/util" --cmd_file="configPkg/compiler.opt" "../source/util/VecMath.cpp"'Finished building: ../source/util/VecMath.cpp'' ''Building target: LinearDeltaCode_v2.0.out''Invoking: ARM Linker'"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=ccs --define=TIVAWARE --diag_wrap=off --diag_warning=225 --diag_warning=255 --display_error_number --gen_func_subsections=on -z -m"LinearDeltaCode_v2.0.map" --heap_size=0 --stack_size=512 -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/lib" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" --reread_libs --display_error_number --diag_wrap=off --warn_sections --xml_link_info="LinearDeltaCode_v2.0_linkInfo.xml" --rom_model -o "LinearDeltaCode_v2.0.out" "./EK_TM4C1294XL.obj" "./empty.obj" "./source/FileIO/GlobalData.obj" "./source/FileIO/config.obj" "./source/FileIO/inih-master/cpp/INIReader.obj" "./source/FileIO/inih-master/ini.obj" "./source/GcodeEngine/GCline.obj" "./source/io/pinout.obj" "./source/motion/DeltaAxis.obj" "./source/motion/DeltaKinematics.obj" "./source/motion/PID.obj" "../source/sysbios/BIOS.obj" "../source/sysbios/m3_Hwi_asm.obj" "../source/sysbios/m3_Hwi_asm_switch.obj" "../source/sysbios/m3_IntrinsicsSupport_asm.obj" "../source/sysbios/m3_TaskSupport_asm.obj" "./source/util/VecMath.obj" "../EK_TM4C1294XL.cmd" -l"configPkg/linker.cmd" -l"C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b/grlib/ccs/Debug/grlib.lib" -l"C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b/usblib/ccs/Debug/usblib.lib" -l"C:/ti/tirtos_tivac_2_16_01_14/products/TivaWare_C_Series-2.1.1.71b/driverlib/ccs/Debug/driverlib.lib" -llibc.a <Linking>error #10056: symbol "ti_sysbios_family_arm_lm4_Timer_start__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_setHookContext__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_getFunc__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_tickReconfig__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_getHookContext__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Queue_get__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Swi_or__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Swi_enabled__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_scheduleNextTick__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Swi_runLoop__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_getTicks__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Queue_enqueue__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_lm4_Timer_getCount__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Queue_put__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_getEnv__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_gates_GateHwi_Instance_init__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_Instance_finalize__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_lm4_Timer_stop__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_getStackInfo__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Swi_getAttrs__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_getIrp__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_lm4_Timer_getStatus__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_processVitalTaskFlag__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Queue_insert__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Queue_prev__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_clearInterrupt__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_post__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_doSwiRestore__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_lm4_Timer_setPeriodMicroSecs__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_getTimerHandle__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_enable__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_getPeriod__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_post__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Swi_restorePri__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_heaps_HeapMem_initPrimary__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_excNmi__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_heaps_HeapMem_restore__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Semaphore_pend__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_heaps_HeapMem_init__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_lm4_Timer_getNumTimers__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_excSvCall__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_removeI__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_dispatchC__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_setArg1__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_getFunc__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_getArg1__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_lm4_Timer_getFreq__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_setFunc__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_sleepTimeout__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Queue_remove__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Semaphore_Instance_finalize__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Semaphore_reset__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_Instance_init__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Swi_raisePri__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_walkQueueDynamic__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_Instance_init__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_BIOS_setCpuFreq__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_allBlockedFunction__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_postInit__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_enter__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Queue_putHead__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Swi_setAttrs__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_switchFromBootStack__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Swi_andn__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_excHardFault__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_getCoreStackInfo__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_disable__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Swi_Module_startup__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_gates_GateMutex_Instance_finalize__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_startup__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Swi_post__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_lm4_Timer_trigger__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_initStack" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Queue_next__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_heaps_HeapMem_getExtendedStats__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_Instance_finalize__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Queue_elemClear__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_Instance_init__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_checkStack" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_getIdleTaskHandle__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_self__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Semaphore_getCount__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_excSetBuffers__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_lm4_Timer_setPeriod__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_startup__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_triggerFunc__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Queue_Instance_init__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_stat__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_setFunc__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Clock_getTickPeriod__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_lm4_Timer_getExpiredCounts__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_getMode__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_lm4_Timer_getExpiredCounts64__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_hal_Hwi_Module_startup__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_excHandler__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_family_arm_m3_Hwi_excUsageFault__I" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Swi_disable__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_BIOS_setThreadType__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"error #10056: symbol "ti_sysbios_knl_Task_disable__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"
error #10056: symbol "ti_sysbios_knl_Intrinsics_maxbit__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>">> Compilation failuremakefile:175: recipe for target 'LinearDeltaCode_v2.0.out' failederror #10056: symbol "ti_sysbios_knl_Swi_Instance_init__E" redefined: first defined in "../source/sysbios/BIOS.obj"; redefined in "C:\CodeDirectory\CCS\LinearDeltaCode_v2.0\src\sysbios\sysbios.aem4f<BIOS.obj>"fatal error #99900: error limit reached; 100 errors detectedgmake: *** [LinearDeltaCode_v2.0.out] Error 1gmake: Target 'all' not remade because of errors.
**** Build Finished ****