Hi,
For my custom board to work, I always have BSP_SDRAM_BANK1_ENABLE set to 0. Since I started using Unified BSP 1.00 , I could no longer be able to download the OS image to my custom board through RNDIS USB, so I went back to the EVM for the baseline.
When setting BSP_SDRAM_BANK1_ENABLE = 1, I could download the image through RNDIS USB and the EVM displayed the shell screen. When setting BSP_SDRAM_BANK1_ENABLE = 0, the OS hang soon after being started. Below are the only output I got when downloading the debug build from platform builder:
Error Reporting Memory Reserved, dump size = 0004b000
Setting up softlog at 0x847b1000 for 0x800 entries
Booting Windows CE version 6.00 for (ARM)
&pTOC = 82df0c1c, pTOC = 82d88544, pTOC->ulRamFree = 82df5000, MemForPT = 00001000
Old or invalid version stamp in kernel structures - starting clean!
Configuring: Primary pages: 6582, Secondary pages: 42987, Filesystem pages = 24784
I appreciate your advice on what changes I need to do to have the EVM works when setting BSP_SDRAM_BANK1_ENABLE = 0.
Thanks,
Luan