Other Parts Discussed in Thread: TPD2S300
In our design we have 2 USB TYpe C ports one is for Communication & power and the other is used for supplementary power (no communication)
1. For the Communication & Power port we intend to use the TI TPD6S300 for the protection circuit.
a) Do we also need a PulseGuard ESD Suppressors - PGB1010603 VBUS lines as well like we have in other USB 2.0 designs or is this covered by the TI TPD6S300 ?
b) We are not using Alternate mode so I am assuming that the SBU1\2 pins on the Type C connected should be left unconnected ? What about the associated pins on the TPD6S300 (C_SBU1\1 & SBU1\2) also they should be left unconnected ?
2. For the supplementary power port, the signals we will be connecting to are the VBUS and the C1\C2 lines. What type of protection would you suggest ? The TI TPD6S300 ? Is this a little over kill since we will not be using the SSTX \ SSRX nor the DP \DN lines ? Would a PulseGuard ESD Suppressors - PGB1010603 on the VBUS lines be sufficient - what the CC lines ?
Best Regards
Shmuel