This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tusb3410+msp430g2231

Other Parts Discussed in Thread: MSP430G2231, TUSB3410

Hi!

I'm trying to connect a msp430g2231 through a tusb3410 to the computer. I've made a board for the tusb, the circuit it is shown in the picture. There you can also see the connection with the msp430. the mcu is in the Launchpad and it has the "Pre-programmed Demo Application - Internal Temperature Measurement" in flash.


the tusb3410 board is recognized by the computer but I can't see any data being transfered



the "STATUS" bar in the serial capture program shown some activity on CTS, DCD, DSR and Ring, however, none of these pins are connected.

With the msp430 conected with the Launchpad as serial port I'm able to see the data stream and the RXD pin in the "status" bar blinking so the mcu it's not the problem.

Any ideas?

Thanks

Juan Ignacio