There is following description about USB_VBUS pin in datasheet page.9.
Yaita / Japan disty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yaita-san,
VBUS is debounced for > 1ms, but only when going from low to high. It is not debounced on a high to low transition. This means that the customer apication could see a false VBUS low event. Can they set VBUS higher in the system or increase capacitance to avoid the noise?
Regards,
JMMN
Hello Yaita-san,
Changing the resistor value should address the issue. Please be aware the USB specification requires 1 uF to 10 uF on the VBUS input to the hub as well, this capacitance may help address the noise spike as well.
Regards,
JMMN