Using TUSB3x10 EEPROM Burner utility, is it possible to configure it to utilize the serial die id number?
If customers use TI vendor ID 0450 and PID 3410, they don't need to change the inf file included in TI VCP driver's package.
So they don't need to pay for Windows driver certification. However VID/PID/Serial number combination must be unique.
If they can use the serial die id, each device should be unique.
Regards
msmn