TMDS181 team,
Can you please let us know if there are internal pull-ups or pull-downs on the I2C_EN/PIN pin (pin 10)? Which mode will apply if the pin is left unconnected?
Thanks,
Darren
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TMDS181 team,
Can you please let us know if there are internal pull-ups or pull-downs on the I2C_EN/PIN pin (pin 10)? Which mode will apply if the pin is left unconnected?
Thanks,
Darren
Hi Moises,
To be more specific, if it'll be OK to use a zero-ohm resistors for A1 and I2C_EN/PIN pins?
On the figures in the section 9.2 (Typical Applications), each the pin is wired to the resistor (pullup or pulldown), similar to the other control pins nearby. This is consistent with the Pin Function table (page 5) where the logic levels for that control pins are defined as (H) Logic high (pin strapped to VCC through 65 kΩ resistor); (L) Logic Low (pin strapped to GND through 65 kΩ resistor); (for mid-level= No connect).
However, there is no mentioning of the resistors for the A1 and I2C_EN/PIN pins in the table. That pins looks more like an ordinary logic inputs that may be wired directly to GND or Vcc or may be driven by a controller's GPIOs.
A resistor usually has the Cost attribute so it'll be interesting to know if it's really necessary.
---
regards,
Igor
Hi Igor,
You could tie to GND if you are sure a change won't be needed, is a high level is needed you have to use 65k.
If I2C_EN is tied to GND, A1 is left floated
Regards