Hello,
We have an application where we have a TFP401APZP powered from a 3.3V supply and I need to drive the _DP input from a 5.0V source.
To protect the _DP input from an over-voltage/current condition I’ve added a series resistor to limit the input current into the _DP pin.
I am relying on the internal ESD diode to clamp the input voltage to a safe level.
However the datasheet does not have a specification on the current capacity of the ESD diodes on these input pins.
Can you help us determine what the maximum current capacity of the internal ESD diode is on the _PD pin on the TFP401APZP?
Thank you, Keith