HI team
TMDS181 was fialed at HF2.1 of HDMI2.0 compliance test.
Would you please let me kwnow what setting could imorove with stand alone mode
or register conrolt with I2C ?
HF2.1 of HDMI2.0 is required to signal level is at least 150mV, but TMDS181 could not meet at thier configuration.
*Using TI EVM(EVM setting is default)
* Test configuration is
HDMI Input --- TMDS181EVM --- HDMI Tx/Rx --- HDMI to HD Base T --- TMDS Rx --- HDMI Tx --- HDMI Out --- Monitor
*HDMI 2.0 Compliance Test reulst
Only failed at HF2.1, othre were OK.
TMDS181:170mV
Other IC : 70mV
・In case of only TMDS181EVM.
120mV, test result is OK.
So, TMDS181 is reguried to adjust settting for thier configuration.
Would you please let me know.your suggetion ?we need to fix by tommorow.
I would appreicate your support.
best regards K.Kanao