Hello
We have designed a board that include the TCA6424A controlled by TM4C123 the micro controller send messages in I2C to the address of 0x22 and 0x23 with no ACK in respond.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
We have designed a board that include the TCA6424A controlled by TM4C123 the micro controller send messages in I2C to the address of 0x22 and 0x23 with no ACK in respond.
The address listed in the datasheet (0x22) is often referred to as a "7-bit address", in other words drop the R/W bit and add a '0' at the front, or right shift and divide by 2.
It is possible that your software needs a 8-bit address as the input.
Read = 0x45
Write = 0x44
Since you have ADDR grounded, the "7-bit address" of 0x23 is not relevant for your application. 0x23 is equivalent to the 8-bit addresses 0x46 (Write) and 0x47 (Read).
I have tried that with no success more then that I wrote a code that send messages to all the addresses in that BUS. the TCA6424A is the only component that connected to that BUS.
There was no respond ACK to my messages.
If that's the case then I will have to see a scope shot showing SCL and SDA clearly during the communication sequence.
If you have an I2C enabled scope that would be great. If not, then I will be able to count the bits if the scope shot is clear enough.