We are using TCA6424A in our application. We have configure 5 pins of port 2 as inputs. Whenever level of input is changed a interrupt is generated. The system functions successfully for a 3-4 days and suddenly TCA6424 stop generating interrupts.
We have an additional device BQ32000 connected on same I2C bus. Which works normal. Also when the problem occurs ports of TCA6424 configure as outputs are working normal.
So problem is that TCA6424 stops generating interrupts. We have conform the same by using an DSO.