Dear All,
・Our customer wants to use TPL0102 with TPS65130.
・TPS65130 uses two sets of partial resistance with the power supply product
that both output the positive voltage and the negative voltage.
http://www.tij.co.jp/product/jp/TPS65130?keyMatch=TPS65130&tisearch=Search-JP-Everything
・When a user adjusts partial pressure resistance of the positive-voltage side
and the negative-voltage side, is the following setting right?
(Single Supply Operation)
[Setting Example]
VDD :5 [V]
VSS :0 [V](GND)
GND :0 [V]
・Or does a user have to set it as follows? (Dual Supply Operation)
[Example of setting]
VDD :2.5[V]
VSS :-2.5[V]
GND :0[V]
Best Regards,
Tsuguhiko Asai