Hello,
I have an automotive circuit with MSP430F5438A and there are some inputs to be given to the MSP from the automobile electronics.
All the inputs will have 12V and for MSP430, they need to be shifted to 3.3V. Also the current in those inputs can be pretty high, ranging from 500mA to 1 or 2A.
Is there any IC that could be used?
I have looked at TLC27L4, CD40109B-Q1.
Can anyone provide an expert opinion on which one to use? Also if any other solutions available??