In the datasheet of this part, it states that
"When the output-enable (OE) input is low, all outputs are placed in the high-impedance state. To ensure the
high-impedance state during power up or power down, OE should be tied to GND through a pulldown resistor;
the minimum value of the resistor is determined by the current-sourcing capability of the driver.
The TXB0104 is designed so that the OE input circuit is supplied by VCCA."
I am currently have VCCA using 3.3V. What is the recommended value for the minimum value of the resistor? Thanks.