Hi,
I am planning to use TXS0206 for interfacing a 1.8V processor with a 3.3V SD card interface. But when I was checking the logic levels between those, I saw conflicts between them.
Processor Logic Level (1.8V):
VIH = 0.65*VCC, VIL = 0.35*VCC ;
VOH = 1.4V, VOL = 0.45V
TXS0206 Logic Level:
VIH = VCC-0.2, VIL = 0.15
VOH = 0.8*VCC, VOL = 0.4V.
SD Logic Level (3.3V):
VIH = 0.625*VCC, VIL = 0.25*VCC
VOH = 0.75*VCC, VOL = 0.125*VCC.
What can I do with this? Please help me out of this.