Hi Team,
I have one urgent issue from automotive customer.
Customer is using TXS0108E for both SPI and I2C, but find that SPI channels have oscillation, after changing to TXB0108, SPI work now, while I2C would then fail as expected.
I checked from some spec and app note, that TXS0108E should work for both open-drain and push-pull application, could TXS0108E be used for SPI ? What should cause the abnormal issue ?
(I was thinking the retrigger of O.S causing the oscillation, but if so, it should also happens even changing to TXB0108, or might be worse, as the O.S timeout is shorter as 10ns, while TXS0108E is 10-30ns)
Thanks.