The ClkRun pins allows the clock signal to be transmitted to the SIM when the SIM is deselected. When would that be useful?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The ClkRun pins allows the clock signal to be transmitted to the SIM when the SIM is deselected. When would that be useful?
Mark,
My understanding is that the purpose of CLKRUNx is for ensuring compatibility with SIM cards that do not support 'Clock Stop'.
Let's take the ISO/IEC 7816-3 standard, which specifies the electrical interface and transmission protocol for these cards.
There is a power saving feature in that specification which is called 'Clock Stop'. This feature allows an interface device to stop transmission of CLK to a SIM card, when data is not expected from that SIM card.
'Clock Stop' is an optional feature for a SIM card. SIM cards that do not support 'Clock Stop' will require continuous reception of CLK. Therefore, the TXS4558 CLKRUN pin must be configured high when connected to a 'Non Clock Stop' SIM card.
Best Regards,
Nirav