Hello!
Should I additionally connect MAX232 (or similar IC) to TMDSDOCK28335 to permit an SCI transmission between TMDSCNCD28335 and a serial port of a PC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
Should I additionally connect MAX232 (or similar IC) to TMDSDOCK28335 to permit an SCI transmission between TMDSCNCD28335 and a serial port of a PC?
Michael,
I am not familiar with that evaluation module. However the features list says that RS232 signal are available on the EVM. Therefore you do not need a MAX232. The RS232 signals from the EVM can be connected to the PC serial port.
Thanks for the reply, Ronald! I have controlSUITE installed and I found the schematics for the F28335 controlCARD here: C:\TI\controlSUITE\development_kits\~controlCARDs\CC2833xHWdevPkg\. When I opened "F28335 controlCARD ZJZ Schematic [R2.2].pdf" I noticed that MAX3221ECPW is used as RS-232 line driver.
Best regards, Michael.