on power up TLK110 will not respond to host via MDIO. Traced it down to JTAG_TRST pin. We have 2.2K pullup but about 30% of boards from current build fail Ethernet test. The only way I can get part to work is to tie JTAG_TRST low or remove external pull-up. Can we have JTAG_TRST pin on TLK110 permanently tied LOW or should it be left floating? Data sheet has no info on how JTAG_TRST should be used. I found couple similar posts on e2e forums but they all went to offline conversations without solution been posted so everyone can see it.