Hello,
I have a question about I2S_WC and I2S_DA output of Ds90UB948.
We are using DS90UB949 and DS90UB948.(dual link)
I want to transmit the I2S master signal of DS90UB949 to DS90UB948
(Using the GPIO6_REG, GPIO7_REG, and GPIO8_REG pins)
I confirmed that I2S_CLK is transferred to DESER by changing AUDIO MODE of 0x54 (BRIDGE_CFG) of UB949 to Local / DVI mode.
However, when I2S Transport Select of 0x12 (Data Path Control) is set to Island transport, I2S_WC and I2S_DA do not appear in DESER.
(It operates only in Data Forward Channel Frame transport mode.)
Our configuration is as follows
DS90UB949
1. 0x12 (data path control) = 0x00
2. 0x1A (data path control2) = 0x00
(no surround mode)
3. 0x30 (SCLK control) = 0x80
(SCLK / WS = 32)
4. 0x54 (BRIDGE_CFG) = 0x2A
3. 0x62 (SPI CONFIG) = 0x01
(for SPI)
DS90UB948
1. 0x43 (HSCC_CTRL) = 0x06
(for SPI)
Here is the question.
1. How can I communicate in I2S island transport mode?
2. We want to transmit the I2S signal with low latency or constant latency.
In the Data Forward Channel Frame mode, the I2S_WC and I2S_DA are too randomly delayed
Is it possible to transmit with a small delay in island transport mode?
If not, how can I do that?