Hello,
I have a design where I am using the TUSB8020B to connect 2 Microchip LAN7801 bridge chips(downstream ports) to a USB3 upstream port.
When I plug the upstream port into a USB2 port, all works as expected - both LAN7801 chips show up in the USB Device Viewer program.
When I plug the upstream port into a USB3 port, I see the 8020 hub as USB2 and USB3, but I see no devices connected to the 8020, either USB2 or USB3.
When plugged into a USB3 port, I have scoped pins 21 and 22 on the 8020 - most of the time those signals are logic high. About every 360ms, there is a 1ms logic low pulse.
Is there a program to communicate with the TUSB8020 over USB??
Any thoughts would be appreciated - Thank you,
Mike