Other Parts Discussed in Thread: PCA9517, DRV10983, TCA9509, , ISO1540, TCA4311A, PCA9306, TCA9406, TXS0102, LSF0102
I2C MASTER SIDE Run At 5V, This is on borad A, 1scl and 1sda are the master,sclo1 and sdao1 are connect to board B.
I2C SLAVE SIDE, This is on borad B,sclo1 and sdao1 are connect to board A,
1scl and 1sda are the SIDEA 1 of ADUM1251, AND connect to PCA9517 SIDE B,
3scl and 3sda are connect to DRV10983 Run at 3.3V。
I wonder if there is some problem in the schematic,
can someone help me to check this ?