Other Parts Discussed in Thread: VCA810
Tool/software: WEBENCH® Design Tools
Hello TI Team,
We are working on project based on visible light communication, for that we have a requirement of trans-impedance amplifier which can convert current into voltage with automatic gain control circuit.
auto gain control is required if receiver circuit(photo-diode) is move within some distance, so we are decided to select IC having part number #ONET4291TA.
Our transmitter will transmit data at 10kHz frequency, hope this device support this frequency for better communication. we already read the datasheet but still have some doubt.
Question:
1) Can this IC receive data without any loss using photo-diode because transmitter which is transmitting light on the photo-diode circuit is in moving within 1 meter?
2) As mentioned in datasheet output is analog and differential, if we want only positive output can we connect negative output with ground?
3) This IC will deliver fix output voltage using internal AGC??
4) if possible share me the reference schematic for the same.