Other Parts Discussed in Thread: TCA9517, PCA9548A, TCA9617B, TCA9801, TCA9509, PCA9306, TCA9803
Hi,
In our design we have an I2C bus where Zynq Ultrascale+ (XCZU9CG-2FFVB1156E) PS is the master, and controls a PLL through an I2C hub(VDD 2.5V). So a level translator TCA9517 was used to do the translation from 1.8V (PS side) to 2.5V (Hub side). Few of the boards were working fine. But, later it was realised, the TCA9517 on side B can translate in range 2.7 to 5.5V. So , we replace dthe part with TCA9617A (TI samples), a sTCA9617 is footprint compatible and has range of 2.2V to 5.5V on side B. But, the I2C bus doesn't seem to work reliably. On changing the IC back to TCA9517, the bus transactions seems okay, but it is not electrically correct. Please help, if the part TCA9617A has any issues? Can TCA9617A be used in place of TCA9517?
Regards,
Rajneesh