Dear all,
I would like to ask about LED operation mode.
Currently our customers are evaluating DP83822IRHBR.
They want to change the behavior of LED_0 to "ON when linking, blinking when communicating (Transmitter or Receiver is active)",
so they have changed from the default setting (Mode1 for LED_0) to Mode2 for LED_0.
When they set BIT5 of PHYCR to 0, the LED works as set, but when doing ping, it takes longer to respond compared to Mode1 of LED_0.
PHYCR.BIT5 =1(default) About 0.1ms for ping response (when LED_0 is Mode1)
↓
PHYCR.BIT5 = 0 About 100ms for ping response (when LED_0 is Mode 2)
As a precaution, I set LED_CFG in Strap and set Mode 2 of LED_0, but in this case, the ping response is 100ms.
Is there any difference in the response speed of ping due to the change of MODE of LED_0?
Also, if there are any conceivable factors, would you please tell me?
Is there any way to change the MODE of LED_0 without slowing down the ping response?
Best Regards,
Y.Ottey