Should we make all the HDMI input (and output) traces the same length, or should those have different lengths based on the RULES of the Eval Board?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Should we make all the HDMI input (and output) traces the same length, or should those have different lengths based on the RULES of the Eval Board?
Thank you!
Hi
Is the TMDS181 being used on the source side or the sink side?
On the source side, the HDMI spec calls for a skew of 0.2 * Tcharacter at TP1 (source connector).
On the sink side, the HDMI spec calls for a skew of 0.2 * Tcharacter + 1.78 ns at TP2 (sink connector). For TMDS181 input, we can tolerate a skew of ~2 * Tcharacter.
A Tcharacter is defined as the time duration of a single TMDS character equal to 10*Tbit.
A Tbit is defined as the time duration of a single TMDS data bit.
Please use the above skew number as a guideline for the trace inter-pair skew. But it does not mean the board should be designed to completely match these skew number. I would still recommend routing the trace length as close to each other as possible.
Thanks
David