I am using a laser diode with the following specs. Is there a TI laser driver that can modulate the intensity from DC up to 250Hz within the specified voltage range. This diode is used for IR illumination.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using a laser diode with the following specs. Is there a TI laser driver that can modulate the intensity from DC up to 250Hz within the specified voltage range. This diode is used for IR illumination.
Justin,
The laser drivers we develop are for communications systems at data rates above 1Gbps. We do not have a laser driver for very low data rates.
Regards,
Alex.