I was looking at the ONET4201LD for a new project. While looking at the datasheet I found the following....
LASER DIODE INTERFACE
The output stage of the ONET4201LD is optimized for driving a 20-Ω load. The combination of a damping
resistor, RD, along with the resistance of the laser diode must be 20 Ω for impedance matching. The suggested
typical value for RD is 6 Ω to 15 Ω. A bypass capacitor of 10 nF placed close to the laser anode also helps to
optimize performance.
In my case, the laser diode that I am planning to use is a FINISAR HFE4192-581 which has a nominal series resistance of 35 ohms.
My question is, will the ONET4201LD have an issue driving this device? Or, is there something that can be done to improve the compatibility?