I have a customer asking the following questions regarding the ONET1151L:
I would like to use ONET1151L as 10G laser driver. The input signal is CML from ASIC which is designed as CML VCSEL laser driver.
Can you please confirm that ONET1151L can directly interface to CML transition?
If this is possible can you let me know the bias voltage (internal) that is used with the ONET1151L since the inputs are AC coupled?
Please let me know if the customer can use CML signals on the input. I am fairly certain that this is possible, but can you send a picture of how you would recommend that the customer configure the inputs so that they could interface this properly?
Thanks for your help with this!
Richard Elmquist