Hello!
I'm currently trying to understand the datasheet of the TLK10232. On page 41, the GLOBAL_CONTROL_1 register (1E.0000) has two entries that go hand in hand.
Bits 14:12 say: PRTAD0 pin selection control. Valid only when 1E.0000 bit 5 is 1. PRDAD0 is used for the assigment specified below ...
Bit 5 says: PRTAD0 pin enable control. 0 = Input pin (PRTAD0) is used for the assignment specified in 1E.0000 bits 14:12 (Default 1'b0). 1 = Input pin (PRTAD0) is not used for the assigment specified in 1E.0000 bits 14:12.
It looks to me that they're claiming the opposite. Did I get it wrong?
Tobias