Hi all,
I have a SN65LVDS93A chip which drive at 100 MHz clock input frequency. I'm using SN65LVDS94 to deserialize the data.
But the data receive on SN65LVDS94 sometimes isn't correct with the source data.
Can the SN65LVDS94 drive at 100MHz frequency. If not, which is compatible receiver with SN65LVDS93A at 100MHz input frequency?
Thank in advance and best regards,