Hello,
My customer has a question about DS32EL0421 / DS32EL0124.
[Background]
They are going to use DS32EL0421 and DS32EL0124 as follows.
・A DS32EL0421 is directly connected to a DS32EL0124 with AC coupling. ---> RS=0 (Remote Sens enabled) and DC_B=0 (DC Balance enabled)
・They connect both with STP cable of the following length.
(a) 5m
(b) 10m
(c) 15m
[Q]
Please tell me the appropriate start-up sequence of these devices.
It is helpful for understand it when you can explain it with the state diagram of the data sheet.
For example ...
(1-a) The 3.3V power supply for DS32EL0124 is powered up.
(1-b) The 3.3V power supply for DS32EL0421 is powered up.
(2-a) The 2.5V power supply for DS32EL0124 is powered up.
(2-b) The 2.5V power supply for DS32EL0421 is powered up.
(3) Set the Configuration pins for DS32EL0421 / DS32EL0124.
(4) Set the Configuration registor for DS32EL0421 / DS32EL0124. (Optional)
(5) Input TX data and TX clock
... and so on ...
Best Regards,
Hiroshi Katsunaga