Customer will use DS92LV18 and SN65LVDS250 below connection.
Are these "cascade" crosspoint switch no problem?
And, is the place of termination resistor correct?
Best regards,
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Customer will use DS92LV18 and SN65LVDS250 below connection.
Are these "cascade" crosspoint switch no problem?
And, is the place of termination resistor correct?
Best regards,
Satoshi
Hello Satoshi,
Take in account that the DS92LV18 is a receiver/transceiver and the SN65LVDS250 is a unidirectional Crosspoint switch.
Also for the LVDS250, 50 ohms termination resistor input is recommended and a 100 ohms termination resistor output is recommended.
Please let me know if further help is needed.
Regards,
Gerardo
Garard-san
Thank you for reply.
Please let me check about termination resister below;
①Are Input / Output termination mean DS92LV18 input and output?
For example, DS92LV18's LVDS input line connect 50Ω and output line connect 100Ω.
Or, is termination resister based on crosspoint switch? (Below image? Red point is termination resister.)
②About input termination, I think that IN+ and IN- connect separately 50Ω to GND, is it correct?
③Is input line necessary termination resister?
Best regards,
Satoshi
Hi,
and quesiont is unused LVDS-input pins of SN65LVDS250.
(Unused pins: 3A,3B and 4A,4B)
Which is better for them?
(open or pullup/down)
best regards