Dears,
My customer wants to use SD65DSI84 to convert MIPI to LVDS and connect with DS90UB905 to the LVDS panel which is DS90UB906 inside.
However, he failed and there is no any display on panel.
While use SN65DSI84 patten as signal source, they can see the patten on panel. It means the trace is OK from SN65DSI84 output to panel.
Another test is using MIPI to RGB888 IC to provide RGB888 signal from same MIPI signal then connect to DS90UB907 and panel, there is no problem with such connection.
My question is, why SN65DSI84 cannot convert same MIPI source to LVDS then pass to panel through DS90UB905?
Does such connection workable or not?
Thanks.