I have two identical serializer boards (I can provide schematic diagram) and I am experiencing problems when I try accessing serializer registers on one of the boards. I am always using the same deserializer board channel for testing the serializer boards, the same I2C access sequence, power supplies look O.K. board is connected to the deserializer board using coaxial cable, deserializer lock is present and stable, and FPD Link signal looks the same with both serializer boards (I can see backchannel low frequency signal and superimposed high frequency forward channel signal). Serializer is using external 48MHz clock (mode pin voltage level is set accordingly). Is there any Link test I could preform (besides BIST) that could help me find what is wrong with the board.