Apologies for not supplying the part number in the specified field. For some reason doing so would allow me to only select "Ethernet" as the targeted forum.
I have a DS100BR111 set up for SMBus Master Mode with an appropriate EEPROM. I am trying to understand how to program that EEPROM so that the DS100BR111 can read from it. I have tried writing the values directly to the EEPROM. That is, EEPROM address 0x00 contains the first value from Table 6 the datasheet (or Table 1 of SNLA228). This does not seem to work as the DONE pin remains high. I can read the register values of DS100BR111 but cannot write to them - I suppose write is disabled until DONE goes low. Further investigation suggests that I need to create a hex file and write that to the EEPROM. Can I write the values of the hex file manually? Can you please elaborate on this procedure?
I checked out SigCon Architect but do not have a USB2ANY device. I will need to program the EEPROM without if possible. Thank you.