Dear support team,
Our customer is studying TCA9535 now.
I've gotten a question regarding TCA9535 from the customer.
So please teach me about it.
Does TCA9535 has the auto increment function of register address?
For example,
after sending the register address as 0x02, if the master sends 6 bytes data continuously,
is it possible to write the data in the registers 0x02 through 0x07?
Or, is it able to write only every two bytes such as 0x02 and 0x03,0x04 and 0x05,0x06 and 0x07?
Also, is it possible to read the 6 bytes data of 0x02 through 0x07, or every two bytes?
Best regards,
M. Tachibana